Browse FAQs

What is the maximum number of CANopen devices that you can have on a island bus when using a STBXBE2100?

Published date: 23 April 2019

Issue:
Maximum number of CANopen devices when using a STBXBE2100.

Product line:
Advantys

Environment:
Advantys Configuration Software

Resolution:
The STBXBE2100 module supports a maximum of 12 standard CANopen devices on an island bus.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.