Technical FAQs

Ask a Question

Is there a 'used references' function in Control Expert (formerly Unity Pro)?

Direct address usage can be viewed in the Configuration screen. Double click on the Local bus - CPU - Configuration - Viewer. Usage can be viewed for Modules, Language and Variables. Choose the Memory Area and the grid will become populated with blue (IO Modules), red (Variables) or green (IEC code usage) lines.




R-1222018

Was this helpful?
What can we do to improve the information ?