Technical FAQs

Ask a Question

What is the conversion of data for a AS-BADU-216 (or AS-BADU-257 configured as a ADU-216) for J or K type thermocouples.

Conversion data depends upon the model of the TSX Compact CPU that is being used in the system.
For PC-E984-258/265/275:

For PC-A984-1XX, E984-24X/251/255:
The values correlate to degrees Celsius X 20 (i.e 100 counts =5 degrees C, 201 counts = 10.5 degrees C, etc.).

Was this helpful?
What can we do to improve the information ?