Technical FAQs

Ask a Question

Can the 8005PR4 be used with the SY/MAX Micro 1 (class 8003) controllers?

Yes. The 8005PR4 Program Loader can be used with the SY/MAX Micro 1(class 8003) controllers; however the user will need to purchase the 8003LC50 cable to interface this model Hand Held Programmer (HHP) to the controller.

Was this helpful?
What can we do to improve the information ?