Technical FAQs

Ask a Question

How do I apply the Concept IEC I_SCALE function block?

The Concept I_SCALE block can only be used with a corresponding system block and a module block.
It is only available for use with the Quantum and Compact platforms. It cannot be used with Momentum.


Legacy KB System (APS) Data: RESL160978 V2.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?