Technical FAQs

Ask a Question

Does the Altivar 61 drive conform to Surge Immunity Standard IEEE C62.41 of 80 joules?

Issue:
Looking for confirmation of Surge Standards on the ATV61 drive. 

Product Line:
ATV61, Altivar 61

Environment:
All catalog numbers, all serial numbers. 

Cause:
Confirming the specifications or standards the drive meets. 

Resolution:
It was confirmed with the Product Engineering team that the ATV61 drives conform to Surge immunity standard, IEC61000-4-5, Level 3 at 2kV.
Was this helpful?
What can we do to improve the information ?