Browse FAQs

NetBotz version 1 and 2 Appliances - MAC Address Ranges

Published date: 29 January 2019

Issue:

NetBotz version 1 and 2 Appliances - MAC Address Ranges

Product Line:

NetBotz

Environment:

NetBotz version 1 and 2

Cause:

Mac address ranges.

Resolution:
 
  • 300
  • 300B
  • 303
  • 310
  • 320
  • 400
  • 420
  • 500 All NetBotz version 1 and 2 monitoring appliances have MAC addresses starting with: 00:02:D3:xx:xx:xx.

    NOTE: NetBotz Central servers have different MAC addresses and they vary depending on the model of NetBotz Central.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.