{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

PowerChute Serial Shutdown or PowerChute Business Edition will not discover Smart-UPS when using 940-0272A cable

Issue,
PowerChute Serial Shutdown or PowerChute Business Edition will not discover the Smart-UPS after connecting to Windows OS using the 940-0272A cable.

Product Line:
PowerChute Business Edition
PowerChute Serial Shutdown

Environment:
All supported Windows OS
Smart-UPS

Cause:
To use the 940-0272A cable with PowerChute Serial Shutdown or PowerChute Business Edition, the Prolific USB to Serial driver must be installed before installing PowerChute.

Solution:
Download the latest Prolific PL2303 driver from http://www.prolific.com.tw/US/ShowProduct.aspx?p_id=225&pcid=41

For Windows Server Core/Hyper-V, the Prolific USB/Serial driver must be downloaded from the Windows Update Catalog onto the Windows Server Core/Hyper-V Server. The cab file must be extracted to local drive and pnputil -i -a ser2pl.inf must be run to install the driver. Windows systems with GUI need to have the Add New Device wizard check Window Update for the driver. Once the driver is installed, reboot the server to register the COM port in the OS.

Schneider Electric Global

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.