Water

Pumps & Fans Control (Industry/Infrastructure)

Pains & drivers

  • In Industry, 70% of electrical consumption is used to turn motors. Of these motors, 33% of them control pump or fan applications.
  • Most pump and fan applications are driven by a DOL solution of SoftStarter. This means that the motor runs at full speed and the flow variation is obtained. The energy consumption falls very little when the flow decreases. At 80% of the nominal flow, the energy consumption remains at 95%. The potential for saving on the installed base is huge.
  • The CEMEP association has made a simulation for the European market. The use of Drive in such applications could save 900 M Euro/year as well as 4 Million tons of CO2/year.
 

How can a customer manage energy more efficiently?

  • To save energy you must:
    - drive the motor with a frequency inverter instead of a contactor or Soft Start
    - remove the restriction device (valve or damper)
  • The AC Inverter allows you to adjust the speed of the Pump or the Fan, and therefore the Flow
  • The result is huge savings compared to conventional solutions:
    - up to 50% for Fan , return on investment for the drive is within one year
    - up to 30 % for a Pump , return on investment within 2 years
 

Solutions or architectures used in the application

 
Solutions or architectures used in the application
A) Solution without Drive
The motor turns at a fixed speed according to the network frequency and the number of poles.
Example : 3600 Rpm for 60 Hz
Motor 2 poles
The only way to adjust the Flow is a restriction device (damper) which generates losses.







B) Energy Saving Solution with Drive
The Drive, which is also called a frequency inverter, lets you vary the frequency and therefore the motor speed, too.
The Flow is directly proportional to the speed.
The damper or valve are no longer required.







C) Energy Consumption with and without Drive
Example for Fan Application

Outlet damper
Variable speed drive
50% of energy saving at 80% of the nominal flow


Example for Pump Application

Control valve
Drive
30% of energy saving at 80% of the nominal flow 

 
 
 
Schneider Electric Solutions
Schneider Electric SolutionsFlexibilityProductivityEnergy cost savingInnovation


Altivar 61

************


W@de W320i, Magelis XBT-N, TeSys U, Altistart 48, Multi 9

******


W@de 320e, Magelis XBT-G, Vijeo Citect, Altivar 61

*****


Altivar 61, Magelis, Vijeo

*********


W@de RTU, Magelis XBT-N, Altivar 61, Multi 9

********


Modicon M340, Advantys STB, FactoryCast, ConneXium, Altivar 61

**********


PowerLogic, Compact NS, Altivar 61

*********


Modicon Premium, Advantys STB, Magelis XBT, Vijeo, Altivar 61, TeSys U

**********


Modicon Quantum, PowerLogic PM650, Altivar 61, Altistart 48, TeSys LT6

**********
 
 
 

To know more 

Requests for Solutions, Products and Services information

Contact your Customer Care Centre now!
 

Success Stories

 
 
  •   ...
  •   ...
  •   More than 50% increase in water ...
More
  •   20% of energy savings, ROI in less than 2 years ...
  •   Cost effective and size optimized solution 30% saved on wiring costs ...
  •   ...
  •   15% energy savings, ROI in less than 3 years ...
  •   ...
  •   ...