Retail
Success Story: RetailForum Malls, Multi Development (Turkey)Being 1![]() I. CUSTOMER ENVIRONMENT / PROJECT CONTEXTCustomer profile:Multi Turkmall is the subsidiary of Multi Corporation, a Netherlands based company in the field of developing, owning and operating shopping centres, offices and mixed-use projects including residential. Their projects are known for their innovative nature, architectural flair and urban connectivity. Multi's projects are often the engine for the regeneration of an entire city or region.
Multi Turkmall has established itself with the 'FORUM' projects. Following the openings of its life-style centres in Izmir (2006), Mersin (2007), Denizli, Trabzon, Aydın (2008), and Istanbul (2009); Multi Turkmall has 16 more Forum Shopping and Life-Style Centre projects under construction. The Multi Corporation manages all its services such as property development, investment, asset management and property management. The design of its malls are by its group T+T Design. They are active in 17 European countries ![]() Customer objective and constraints:Multi development ownes and operates all its properties hence keeps a keen eye on CAPEX and OPEX. Its inhouse design team micro-specifies the engineering structure, hence quality and service factors are quintessential.Since they have an inbred Facility Management team which has energy services, the analysis of monitored information from a Power and BMS front is important. This also creates a need for a single vendor system for support. The mall also preferred tenant metering over W.A.G.E.S. and was keen to have monitoring of both Medium and Low Voltage solutions alongside BMS solutions. The Multi Development further to the construction of their malls plan to integrate the energy modelling of all their malls and have a common database for real-time information onto a single webstation and hence all devices needs to be IP capable. Having retail presence in more than 17 countries means that the architecture has to be open-based to suit its international design strategies. Schneider Electric was chosed as the solution provider in view of all the above information. II. SOLUTION IMPLEMENTATIONImplementation methodology (main phases):The construction of FORUM malls featured similar strategies in construction and development:Phase 1: Study of Lighting and HVAC needs with reference to customers design requirements and stores available. Study of power consumption and load study for application of load-shedding schemes Phase 2: Implementation of the first-ever single point integration of both Power and BMS monitoring, control to one BMS workstation via TCP/ IP. This meant the convergence of HVAC applications, Lighting Control, Fire Detection, Access Control, CCTV solutions, Energy Metering, Power Quality and Core Power solutions analysis and monitoring to a single computer. Phase 3: Implementation of Load-Shedding solution via SCADA interface into the Medium and Low Voltage power solutions. Integration of Power Quality solutions to cater to dynamic power requirements of the Malls Phase 4: Tenant metering over W.A.G.E.S parameters, analysis of energy usage over faciity manegement softwares to forecast energy requirement needs and optimization of devices to truly make the FORUM malls 'sustainable' Phase 5: Energy Services in process. All devices followed an open-architecture of design Duration:This is an ongoing project as Multi-Turk Development wishes to construct 16 more malls in the region of Turkey with 5 already constructed.Solution overview (services, products, systems, architectures...):![]() III. RESULTS / ACHIEVEMENTCustomer benefits:Schneider Electric ensured the customers satisfaction and completed the provision of energy management solutions for 5 FORUM malls in Turkey and assist in building the other 16 malls in the pipeline.The customer (Multi Development) well satisfied with Schneider Electric has asked them to asist further in energy optimization services and strategies for implementing a unique remote monitoring strategy for all the 16 malls from a single venue for Facility Management. Schneider Electric differentiating values VS competitors:The ability to truly understand what makes Energy:1) Safe: By having PLC's work seamlessly with BMS system for Power Management and Load Shedding 2) Reliable: By having the energy meters give real-time data via TCP/ IP network for authorized parties to access 3) Productive: By having a W.A.G.E.S. tenant monitoring system which can customize financial instruments to satisfy all stakeholders 4) Efficient: By installing sensors and meters on all energy access points 5) Green: By simply being Energy Efficienct
Solution breakdownMain services:
|