A complete solution that provides easy customized access to electricity parameters of MV or LV switchboards through the Intranet and web pages.
Value proposition
Up to 15% time and cost saving thanks to: - Immediate access to diagnosis maintenance information - Simplification of interfaces between products - Continuous monitoring of quality and cost of power - Reduce training for users
Differentiation factors
Taking advantage of predefined web pages embedded in the panel, any authorised user regardless of their position - electrician, maintenance, manufacturing, site manager - can view valuable electrical information to save energy, avoid power outages or better manage the electrical asset.
This solution includes delivering MV and LV power equipment that is ready to be plugged into the end-user's Intranet site. Access to the power equipment is done with Internet Explorer.
This solution remains highly upgradeable. It can be considered as the basis for more advanced solutions to improve energy management one step further.
Main characteristics
To know more
Requests for Solutions, Products and Services information