In hospitals, intensive care units or operation rooms are extremely critical and patient life may be at risk.
New hospitals need to work with a valuable and effective partner who can offer the best innovative solution to electrical distribution at the best value: quick and easy installation.
Hospitals managers need partners that can audit the installation, build a consistent and comprehensive architecture to deliver maximum uptime.
Solution in brief
A consistent architecture for addressing key installation concerns and maximize uptime.
Value proposition
Compliance with standards
Availability of energy, continuity of service throughout the life cycle of the hospital
Differentiation factors
One supplier for all key components of the electrical architecture. As a consequence, responsibility is known and it is easier to detect problems and fix them because there is a single point of contact.
Quality of products
Ability to build reliability study, audits...
Solution architecture
To know more
Requests for Solutions, Products and Services information
Success Stories
...
Solution breakdown
Main Products - SM6 - MV/LV transformers - Okken - Prisma - UPS - Powerlogic, IONE, Power factor correction, Vigilohm, Automatic Transfer Switches..