RoHS Compliance
 
 
 

European Union : FAQ

Question 7: What are the thresholds below which it can be considered that a product complies with the RoHS directive ?

 
 

The thresholds to be allowed for are 0.1% by weight for lead, mercury, hexavalent chromium and PBBs and PBDEs. It is 0.01% by weight for cadmium, the homogeneous material in which the substance is located.