With conventional electrical installations, you have to determine in advance how and where your building’s switching systems will be installed, before construction even commences. But with KNX from Schneider Electric, you can keep your options open. That’s because most things in the system can be changed or extended at any time – without the usual mess and without laying new cables.
In addition, all building technology devices and installations are connected via a single bus line. The bus line is laid in parallel to the 230 V power supply.
When you activate a sensor (for example, a pushbutton), an actuator (e.g. the roller shutter control) will carry out all the switching commands required.
The assignment between the devices must be configured with the ETS-Software.
|