KNX system

IP-Router

 
 
The KNX/IP router enables telegrams to be forwarded between different lines via LAN (IP) as a rapid backbone.

The device can additionally serve as a programming interface in order to connect a PC with the KNX bus (e.g. for ETS programming with suitable ETS). The IP address can be assigned dynamically via a DHCP server or via manual configuration (ETS parameter).

The device operates in accordance with the KNXnet / IP specification using Core, device management, tunnelling and routing.
The KNX/IP router forwards telegrams in both directions whilst taking a filter table into account and can buffer up to 150 telegrams.
   
 
 
 
 
 

Available products

Coupler REG-K

KNX IP-Router REG-K

MTN680204

MTN680329

This image can't be displayed
This image can't be displayed