KNX system

KNX system components

 
 

KNX comprises a two-wire bus line and the connected bus-compatible installation devices, such as sensors, actuators and system components.

System devices and components are required for the fundamental system functions. These are essentially power supplies for generating the bus voltage, couplers for connecting bus section.

 
This image can't be displayed
This image can't be displayed