KNX system

Switch actuators

 
 

The Schneider Electric actuators fulfill all your customers' wishes. Schneider Electric has the right switch actuators for every application, which distinguish themselves by their simple installation.

The switch actuators are available as 2-gang, 4-gang, 8-gang and 12-gang version. Whether it be small or large loads, no problem!

The switch actuators are available from 6 A to 16 A with electrical or mechanic manual mode.
Furthermore, selected actuators have current detection, which detects the load current of each channel, an operating hours counter, a switch-on counter and an integrated power meter.

   
 
 
 
 
 

Available products

KNX sw.act. REG-K/8x230/6

KNX sw.act. REG-K/2x/10 w.man.mode

KNX sw.act.REG-K/4x/10 w.man.mode

KNX sw.act.REG-K/8x/10 w.man.mode

KNX sw.act.REG-K/12x/10 w.man.mode

KNX sw.act.REG-K/2X230/16 w.man.mode

KNX sw.act.REG-K/4X230/16 w.man.mode

KNX sw.act.REG-K/8x230/16 w.man.mode

KNX sw.act.REG-K/12x230/16 w.man.mode

KNX switch act.REG-K 2g w.curr.detec.

KNX switch act.REG-K 4g w.curr.detec.

KNX switch act.REG-K 8g w.curr.detec.

KNX switch act.REG-K 12 g w.curr.detec.

KNX sw.act.FM/230/16

MTN646808

MTN649202

MTN649204

MTN649208

MTN649212

MTN647393

MTN647593

MTN647893

MTN648493

MTN647395

MTN647595

MTN647895

MTN648495

MTN629993

This image can't be displayed
This image can't be displayed