Large buildings such as hotels, office blocks or clinics are faced with the challenge of controlling heating, air conditioning and ventilation for efficiency and comfort.
Above all, operation needs to be made as simple as possible for users. An intelligent, compact solution for this: the KNX fan coil actuator from Schneider Electric.
This allows, heating, air-conditioning and ventilation systems to be controlled centrally and conveniently.
All of this is done with a single unit via multi-function push-buttons with a room temperature control unit from the Schneider Electric switch range.
|