KNX system

Blind and switch actuators

 
 

The blind/switch actuators are especially practical, and available for 8-blind/16-switch setups or for 12-blind/24-switch setups.

Each channel can be operated either as a blind channel or as a switching channel. In the "Switching" channel operating mode, one blind channel is divided into two equal switching channels. The channels must be toggled at the device itself and in the ETS.

It is not possible to invert the blind and switching channels. If the software and hardware configurations of the parameterized channels are not aligned, the relays of the affected channels are immediately opened and disabled.

   
 
 
 
 
 

Available products

KNX bli.act. REG-K/4x/6

Bli.act. REG-K/4x/24V w.man.mode

KNX rol.shut.act.REG-K/4x/10 w.man.mode

KNX bli.act.REG-K/2x/10 w.man.mode

KNX bli.act.REG-K/4x/10 w.man.mode

KNX bli.act.REG-K/8x/10 w.man.mode

KNX bl.sw.act.REG-K/8x/16/10 w.man.mode

KNX bl.sw.act.REG-K/12x/24x/10 w.man.mo

Weather combi sen. / DCF77 bk

Weather station REG-K/4-gang lgr

MTN646704

MTN648704

MTN649704

MTN649802

MTN649804

MTN649808

MTN649908

MTN649912

MTN663692

MTN682991

This image can't be displayed
This image can't be displayed