| KNX consists of a twin-core bus line and bus-compatible installation devices such as sensors, actuators and system components, that are connected to it.
Actuators receive data telegrams and convert these e.g. into switching or dimming signals. Actuators are selected depending on the required application and consist of a bus coupler and an application module with the corresponding application program. The application programs are part of the Schneider Electric product database.
They are loaded into the devices together with the project design and commissioning software ETS via the serial interface of a PC and the bus.
|