System Integrators dedicated area
System Platform & Engineering tools – Unity Pro
For software productivity “All-in-one” easy to use softwareUnity Pro makes best use of the graphic and context-sensitive interfaces of Windows XP® and Windows 2000®. Five IEC61131-3 languages to mix as you wishUnity Pro offers the five IEC61131-3 languages as standard. Each section of code can be programmed in the language of your choice, best adapted to each processing operation. All edit, debugging and operation tools are accessible whatever the language used.
Compatibility with existing applicationsIntegrated solutions or converters are proposed for migration of existing applications as a function of the initial software platform: All the advantages of standardisationBenefit from a complete set of functions and tools enabling modelling of application structure on your machine or process structure. Time saving by reuseTested and qualified, your standards reduce on-site development and installation Improved quality assuredThe integrated programmable controller simulator faithfully reproduces behaviour Reduced downtimeUnity Pro provides an integrated library of application diagnostic DFBs, which
Precise for control open for collaboration SFC View: SFC programme monitoringPerfectly complementing Unity Pro, Unity SFC View assures monitoring and control of programme SFC sequences. In particular, it traces and indicates faults in execution. Unity SFC View functions on any ActiveX compatible HMI. Unity Developer’s EditionWith UDE, Unity is enhanced by specialised software for IT developers in VBA, VB or C++. It offers access to all Unity Pro software server objects for development of tailor-made solutions such as creation of interfaces with an electrical CAD or application automatic generator. The Want to know more?
|