Technical FAQs

Ask a Question

What issues does the firmware version 1.66 and version 1.67 for the 140NOC78x00 module fix?

Title
Firmware version 1.66 and version 1.67 for the 140NOC78x00 module
 
Issue
Firmware version 1.66 and version 1.67 for the 140NOC78x00 module
 
Product Line
Quantum 140NOC78x00
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 Firmware version 1.66 for the 140NOC78x00 module fixes the issue where Hot Standby CPU swap-overs eventually causes 140NOC78x Port502 Client and/or Server to stop responding.
A reboot was required to recover.

Firmware version 1.67 for the 140NOC78x00 module fixes the issue when using FDR, .prm files transferred to the 140NOC78x00 are not automatically synchronized between primary and standby NOC's in a Hot Standby system.

Firmware release note attached.
Was this helpful?
What can we do to improve the information ?