Technical FAQs

Ask a Question

Can the M580 programatically change it's IP Address?


Title
M580 IP Address
 
Issue
M580 IP Address
 
Product Line
M580 PAC
 
Environment
Unity pro
 
Cause
N/A
 
Resolution
 The M580 can not programatically change it's IP Address. The M580 does not support the SEND_REQ function used to perform the IP address change. 
 
Was this helpful?
What can we do to improve the information ?