Technical FAQs

Ask a Question

Does the M580 PAC support the IEC61850 protocol?

Title
M580 PAC and the IEC61850 protocol
 
Issue
M580 PAC and the IEC61850 protocol
 
Product Line
M580
 
Environment
Unity Pro 10 or higher
 
Cause
N/A
 
Resolution
 The M580 PAC does support the IEC61850 protocol. 
The Modicon M580 using Unity 12, supports the IEC61850 protocol through the use of the BMENOP0300 module.
The main purpose of the BMENOP0300 module is to provide connection with IEC 61850 IED devices as well as device management software that utilizes the IEC 61850 standard.
The BMENOP0300 module is mounted on the local rack and supports communication as:
 IEC 61850 server
 IEC 61850 client
 GOOSE publisher
 GOOSE subscriber
 Modbus TCP server and client
 
Was this helpful?
What can we do to improve the information ?