Technical FAQs

Ask a Question

What is the difference between the 140CPU434-12A and the 140CPU434-12U ?



Answer: The difference between the two CPU's is in the firmware. The 140CPU434-12A has a Concept OS . The CPU434-12U uses a Unity OS




R-6-30-17
 
Was this helpful?
What can we do to improve the information ?