Technical FAQs

Ask a Question

What Windows Operating Systems does Unity DIF v8.0 support?

Unity DIF v8.0 is compatible with the following Windows Operating systems:
-----Windows XP
-----Windows 7 (32 & 64 bit)
-----Windows 8 (32 & 64 bit)
-----Windows Server 2008 R2 (64 bit)

Was this helpful?
What can we do to improve the information ?