Technical FAQs

Ask a Question

Which version of M580 Hot Standby processor will support Quantum I/O?

Issue:  Specifications

Product Line:
M580

Environment: N/A

Cause: N/A

Answer:  The BMEH584040 & BMEH586040 will support 16 and 31 drops of Quantum ERIO. There is no Quantum ERIO support on the BMEH582040.
               


 
Was this helpful?
What can we do to improve the information ?