Technical FAQs

Ask a Question

Does the Magelis Box/Panel PC have DOS drivers to support RS485 communications?

Issue:
Does the Magelis Box/Panel PC have DOS drivers to support RS485 communications?

Product Line:
Magelis Box PC, Magelis Panel PC

Environment:


Cause:


Resolution:
There is no driver for RS485 mode in DOS. The interface works like any standard UART COM interface without a driver. The necessary RTS framing for sending and receiving in RS485 mode has to be implemented in the application driving the interface.
Was this helpful?
What can we do to improve the information ?