Technical FAQs

Ask a Question

Does the Quantum remote I/O system support redundant I/O?

NO. The Quantum will only support single CRA modules in a drop, it will support redundant cabling with the CRP932 and the CRA932.
Was this helpful?
What can we do to improve the information ?