Technical FAQs

Ask a Question

How can Unity Pro error "Wrong form of the export from Concept" be corrected?

Issue:
   Error importing Concept .ASC file into Unity Pro.

Product Line:
   Unity Pro
   Concept 

Reason:
    The wrong export option was chosen when exporting the project out of Concept programming software.
Usually, the user has selected "Project with used DFBs (Re-Connect to Equal)"

Resolution:
    The Concept project must be reexported out of Concept using the first option, "Project with used DFBs".
This .ASC file can then be imported into Unity Pro programming software.

 
Was this helpful?
What can we do to improve the information ?