Technical FAQs

Ask a Question

How do you check the firmware version of a 140NOE771x1 module?


Title
140NOE771x1 module firmware version
 
Issue
140NOE771x1 module firmware version
 
Product Line
Quantum
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
To check the firmware version, please log on to the 140NOE771x1 module webpages.
Select the Diagnostics heading and then select Properties from the left hand menu window.
The Properties page displays the versions of the Exec, Kernel, Web Server, Web Pages and the Physical Media:
 
Was this helpful?
What can we do to improve the information ?