Technical FAQs

Ask a Question

Does the M238/M258 support the 115200 baudrate for Modbus RTU using Modbus Manager in Somachine?

Issue:
Does the M238/M258 support the 115200 baudrate for Modbus RTU using Modbus Manager in Somachine?

Product Line:
TM238, TM258, baud rate, 

Environment:


Cause:


Resolution:
M258 and M238 controllers does NOT support 115200 baudrate for Modbus RTU.  The maximum baudrate it supports is 38400.
Was this helpful?
What can we do to improve the information ?