Technical FAQs

Ask a Question

Can Unity open an 884A PLC program ?

No. Unity Pro cannot open or convert an 884A PLC program. The 800 series IO can migrate to a Unity application
but the program cannot because it uses a unique instruction set. An 884A program would have to be re-written.
Was this helpful?
What can we do to improve the information ?