Technical FAQs

Ask a Question

What is the communications cable between the Magelis HMIGTO series and the TSX Premium controller?

Issue:
What is the communications cable between the Magelis HMIGTO and the TSX Premium controller?

Product Line:
HMIGTO, TSXP57

Environment:


Cause:


Resolution:
The communications cable between the Magelis HMIGTO series to a TSX Premium is XBTZ9780.  The HMIGTO will use COM2 for RS485 communications.
Was this helpful?
What can we do to improve the information ?