Technical FAQs

Ask a Question

What could have caused the Magelis HMIGTO to crash with the following error: Application has halted due to: Out of Thread Handles (email sender-60) KAOscore : PortableThread.cpp : line 76?

Issue:
What could have caused the Magelis HMIGTO to crash with the following error: Application has halted due to: Out of Thread Handles (email sender-60) KAOscore : PortableThread.cpp : line 76?

Product Line:
Vijeo Designer, email, Magelis, XBTGT, HMIGTO, HMISTU

Environment:


Cause:


Resolution:
If the emails were trying to send out while the network was down.  It keeps retrying to a point of overflow.  One recommendation would be to reduce the retry count in the email settings of the target property.
Was this helpful?
What can we do to improve the information ?