Technical FAQs

Ask a Question

What M580 PAC processors supports Quantum Ethernet RemoteIO drops?

Title
 M580 PAC processors that support Quantum Ethernet RemoteIO drops
 
Issue
 M580 PAC processors that support Quantum Ethernet RemoteIO drops
 
Product Line
M580 PAC
 
Environment
Unity Pro 11 (with HF1)
 
Cause
N/A
 
Resolution
 The Quantum Ethernet Remote IO drops using the 140CRA31200 module is supported for BMEP584040 (requires firmware version 2.1), BMEP585040, BMEP586040, BMEH584040,  and BMEH586040.
The configuration of Quantum Ethernet Remote IO drops using the 140CRA31200 module requires programming the M580 PAC with Unity 11 (with HF1) or higher.
 
Was this helpful?
What can we do to improve the information ?