Technical FAQs

Ask a Question

It is possible to upgrade OFS to V3.50 and maintain the authorization with the Vijeo Citect USB key?


It is not possible to upgrade OFS to V3.50 and maintain the authorization with the Vijeo Citect USB key.

You can upgrade Vijeo Citect to the latest version (2015) which comes with OFS V3.50.

 
Was this helpful?
What can we do to improve the information ?