Technical FAQs

Ask a Question

What target to I select for the HMIBMUHI29D2801 in the current version of Vijeo Designer (v6.2)?

Issue:
What target to I select for the HMIBMUHI29D2801 in the current version of Vijeo Designer (v6.2)?

Product Line:
HMIBM Modular Box PC, HMIDM Modular Display

Environment:


Cause:


Resolution:
In the current version of Vijeo Designer v6.2 SP3.1, HMIBMUHI29D2801 is not in the picklist and standard PC Runtime will be used instead.

It not until SP4.1, which will be available in June 2016, will have the capability to select it as Magelis iPC Runtime.
 
Was this helpful?
What can we do to improve the information ?