Technical FAQs

Ask a Question

Do the Quantum processors have the 10 second connection timeout period ?

Title
Quantum TCP Timeout
 
Issue
Quantum TCP default timeout period
 
Product Line
Quantum
 
Environment
Unity Pro 10
 
Cause
N/A
 
Resolution
 The Quantum processors do not have the 10 second default connection timeout period that was incorporated in to the Concept/Proworx Momentum PLCs.
Was this helpful?
What can we do to improve the information ?