Technical FAQs

Ask a Question

Error 6003 when communicating from a legacy Momentum M1E to an M340 BMXNOE01x0 module.

It appears that the BMXNOE01X0 has an isssue the first time (and only the first time) that the M1E start reusing port numbers. The NOE responds with a invalid sequence number however the data it responds with is valid data and the M1E accepts the data but indicated an issue with the packet..  (Error 6003)  However, from that point forward the NOE corrects itself and the remaining transactions are normal. 
Was this helpful?
What can we do to improve the information ?