Technical FAQs

Ask a Question

What is the suggested replacement for the 19-inch iDisplay, MPCYT90NAN00N?

Issue:
What is the suggested replacement for the 19-inch iDisplay, MPCYT90NAN00N?

Product Line:
iDisplay

Environment:


Cause:


Resolution:
The suggested replacement for MPCYT90NAN00N is HMIDID73DTD1 iDisplay monitor and HMIYAD1915D1 panel cut out adapter.  Keep in mind that the replacement is a 15-inch iDisplay.  If you are replacing an existing 19--inch, you will require a panel cut-out adapter.
Was this helpful?
What can we do to improve the information ?