Technical FAQs

Ask a Question

What Protocols are Supported with ION8650 Cellular Modem

Customer would like to know what protocols are available via the cellular modem connection of an ION8650 meter

Product Line
ION8650 A/B/C

Meter communication

The following protocols can be used to communicate with a cellular modem:
  1. Modbus TCP
  2. DNP V3.00
  3. ION
Was this helpful?
What can we do to improve the information ?