Technical FAQs

Ask a Question

What causes Vijeo Designer Data Manager software to error: cannot connect to the specified target, when trying to connect to the Magelis?

Issue:
What causes Vijeo Designer Data Manager software to error: cannot connect to the specified target, when trying to connect to the Magelis?

Product Line:
"cannot connect to the specified target"

Environment:


Cause:


Resolution:
One possible cause of this error is that Data Manager security is set for deny access.  Go to Environment -> Security, "Data Manager Security" under the Property Inspector change the option to either anonymous or use security (see below).  



Then download and check the box to delete all Runtime Data.

 
Was this helpful?
What can we do to improve the information ?