Technical FAQs

Ask a Question

Do any of the Schneider Electric EthernetIP interface modules or PLC platforms support the CIP Sync protocol?

No. The CIP Sync protocol is Not supported by Schneider Electric PLC platforms.

CIP Sync
CIP Sync provides the increased control coordination needed for control applications where absolute time synchronization is vital to achieve real-time synchronization between distributed intelligent devices and systems. CIP Sync™ is compliant with IEEE-1588™ standard, and allows synchronization accuracy between two devices of fewer than 100 nanoseconds. Real-time synchronization can be achieved over conventional 100Mbps, Ethernet systems with a switch-based architecture.

Was this helpful?
What can we do to improve the information ?