Technical FAQs

Ask a Question

Preventa XU - In the IP69K XUSL4E or XUSL2E light curtain versions using a protection tube, what is the distance between the 1st beam and the IP69K tube extremity?

Please find attached a drawing indicating the distance between the curtain into the tube, and the tube extremity, in the XUSL4E(2E)**WC or XUSL4E(2E)**WH versions, using a IP69K sealed protection tube.

Was this helpful?
What can we do to improve the information ?