Technical FAQs

Ask a Question

Is it possible to have multiple ProWORX 32 users logged onto the same PLC simultaneously with each user having the same ability to make edits?

ProWORX 32 doesn't allow multiple PC's to log onto the same PLC simultaneously. When the second user tries to log onto the same PLC with ProWORX 32 they will get message - "Failed to Login to PLC". 

Was this helpful?
What can we do to improve the information ?