Technical FAQs

Ask a Question

What are the characteristics of the Momentum M1E ethernet port?

Title
Characteristics of the Momentum M1E ethernet port?
 
Issue
Characteristics of the Momentum M1E ethernet port?
 
Product Line
Momentum
 
Environment
Concept Proworx
 
Cause
N/A
 
Resolution
The Concept/ Proworx  based M1E Momentum processors are 10 meg half duplex. When connected to a switch, you do not eliminate collisions. As the M1 being half duplex, and the Ethernet switch negotiating a matched 10 Mbs half duplex connection, this remains a collision diameter network of 2 devices. Either the half duplex device can transmit, or the switch can transmit, but not both simultaneously. Only full duplex devices can communicate simultaneously with Ethernet full duplex capable switches.

 
Was this helpful?
What can we do to improve the information ?