Technical FAQs

Ask a Question

Can a Quantum Ethernet port be connected to a 10/100/1000 auto-negotiate switch port?

Title
Quantum Ethernet auto-negotiate switch port
 
Issue
Quantum Ethernet port connection to a 10/100/1000 auto-negotiate switch port
 
Product Line
Quantum
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 A Quantum Ethernet port can not be connected to a 10/100/1000 Auto-negotiate switch port. The Quantum Ethernet port only supports a 10/100 Auto-negotiate port on a switch
Was this helpful?
What can we do to improve the information ?