Technical FAQs

Ask a Question

Why do I get the following error? '=SoMachine V4.1SP2_4.1.0:1_15.12.16.02.seco'.

If you get the following error while installing SP2 for SoMachine V4.1:  '=SoMachine V4.1SP2_4.1.0:1_15.12.16.02.seco'. Make sure you type the name correctly, and then try again.

You need to modify the Environment Variables path.  Right-click on My Computer and select Proterties.  Click on Advanced system settings and Environment Variables under the Advanced tab.
Select Path under Systems Variables and edit the path.  Add C:\Windows\system32\

Error when trying to install SP2.


Add the command WINDOWS\system32 to the path in Windows Environment Variable.

Was this helpful?
What can we do to improve the information ?