Technical FAQs

Ask a Question

It is possible to use the Vijeo Designer included with SoMachine V4.1 in standalone mode to download an application to an HMISTU?

The Demo / limited version of Vijeo Designer can be used to download an HMI application to the Magelis HMISTU. But not when it is installed with SoMachine V4.1.

If you have installed SoMachine V4.1 and want to run Vijeo Designer in Standalone mode you must register Vijeo Designer or install it on a different computer without SoMachine
Was this helpful?
What can we do to improve the information ?